This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28M35的Blinky程序在C28的FLASH中无法运行



使用的是示例的Blinky程序D_blinkly_dc_c28 和 D_blinkly_dc_m3。在M3侧是完全可以正常运行。C28侧在RAM模式下也可以单独运行。但是在FLASH中,就无法运行。

在Debug模式下,如果我同时运行M3的程序和C28的程序,M3的程序会停留在IPCMtoCBootControlSystem 函数,而C28的Debug中,单步运行时C28不是正常单步,而是跳跃式的。

截图如下: