This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于利用GUI实时观测内部变量



1.GUI的实时通信是否与仿真器有关?
我们实验室最早使用的是XDS510的仿真器,IDE环境是CCS3.3,当时发现510只是准实时仿真器,似乎无法实时交换数据。目前使用CCS5.4,对于28335,TI推荐的仿真器为XDS100V2,但我们目前还没有找到关于实时性的说明文档,不知道仿真器对于实时性的影响到底有多大,XDS100V2能否将数据实时回传。

2.由于电机程序调试不能设断点,需要实时观测多个变量。目前是用DA实现该功能的,28335通过SPI总线将数据传给一个4通道的DA芯片,DAC7714再将4个变量以电压的形式输出,并由示波器观测记录。但示波器一次只能观测4个变量,所以需要用其他办法。我不知道GUI的方法能不能保证实时性,同时观测16个变量,在时间上能够同步么?

3.XDS560V2的trace功能是什么?与实时传输数据有关系么?
在XDS560V2的介绍上总是说它具有trace功能,但都没有具体说这个功能怎么用。而且在CCS3.3中提到过RTDX,但在新版本的CCCS中没有看到,这两者有关系么?28335支持支持trace么?您能介绍几个讲的详细的文档么?


4.GUI Composer和GUI Composer Runtime
我搜索了一下GUI Composer,关于这个功能的介绍不是太多,在网页http://processors.wiki.ti.com/index.php/Category:GUI_Composer有一些信息,但不是很多。有些疑问,A)既然网页上说GUI Composer包含在CCS5.3以上的版本中,那为什么还会给出单独的GUI Composer Runtime下载包?
B)网页上给出了一个建立GUI应用的tutorial,但是比较简单,想麻烦问问您有没有更为详细的资料,讲解如何使用GUI工具?谢谢