Part Number: TMS320F280049C
使用的开发板,每次都停在// Error enabling the DC-DC module
//
ESTOP0;这
开发板无法初始化DCDC模块输出1.2V电压吗?
例程里的buffdac_ex1_enable,没做任何修改

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F280049C
使用的开发板,每次都停在// Error enabling the DC-DC module
//
ESTOP0;这
开发板无法初始化DCDC模块输出1.2V电压吗?
例程里的buffdac_ex1_enable,没做任何修改

Hi,
LaunchPad针对这一块没有做硬件上的设计,所以DC-DC模块会使能失败。
使用内部DC-DC模块生成的1.2V电压需要外部连接到VDD电源轨,还需要外部电感和电容配合,同时VREGENZ也要下拉到VSS(GND):
-
VSW是GPIO23,VFBSW是GPIO22。相关内容请查看
zhcsgy3g_TMS320F28004x 实时微控制器 datasheet (Rev. G)的第74页7.9.1.2.6 内部 1.2V 开关稳压器(直流/直流)以及
sprui33f_TMS320F28004x Real-Time Microcontrollers Technical Reference Manual (Rev. F)的第81页3.2.1 Internal 1.2-V Switching Regulator (DC-DC)