This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于28335 GPIO操作速度疑问

哪位大侠帮忙解释下,将28335GPIO设置为IO输出后通过程序置位相应翻转寄存器来产生方波,最大可产生多少频率的波形?查过GPIO的数据手册没有查到相关介绍。

谢谢!

  • 如下:

     

    使用时不要用GPIO Data Register,用GPIO Data Set Register和GPIO Data Clear Register寄存器

  • 最好不要直接用IO功能来产生方波,那样方波的占空比和频率很难准确控制,如果在定时器中产生则相对好些,但定时器中断依旧是对IO取反输出方波占用了CPU资源,如果只是输出方波而不计数最好用PWM模块采用递减/递减方式产生对称方波,如果选择不中断几乎无CPU开销!