将定时器2的PWM输出作为定时器4的时钟输入(硬链接)
GpioMuxRegs.GPAQUAL.all=0x0000;
GpioMuxRegs.GPBQUAL.all=0x0000;
问题:
将捕获到得定时器2的值作为低16位,捕获的定时器4的值作为高16位,发现当低16位捕获到得数据为0附近的较小值时(比如0或1)其高16位捕获到得值还没有加1,及还没有捕获到定时器2的进位!
请问这会是什么问题引起的!定时器对外部时钟除了GPBQUAL寄存器能滤波还有其他的滤波吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
将定时器2的PWM输出作为定时器4的时钟输入(硬链接)
GpioMuxRegs.GPAQUAL.all=0x0000;
GpioMuxRegs.GPBQUAL.all=0x0000;
问题:
将捕获到得定时器2的值作为低16位,捕获的定时器4的值作为高16位,发现当低16位捕获到得数据为0附近的较小值时(比如0或1)其高16位捕获到得值还没有加1,及还没有捕获到定时器2的进位!
请问这会是什么问题引起的!定时器对外部时钟除了GPBQUAL寄存器能滤波还有其他的滤波吗?
我使用的是2812芯片,使用CAP1和CAP5捕获上升沿,CAP1使用定时器2,CAP5使用定时器4,定时器2的周期为0x7FFF,比较寄存器为0x4000,定时器2使用60M的内部时钟,定时器4的时钟使用外部时钟,及72脚TCLKINB
将T2PWM(104脚)和TCLKINB连接,想利用上述方案实现一个31位的捕获!及当CAP5进入捕获中断时同时读出其16位和CAP1的低15位!但实际情况是当CAP1的捕获值为0附近的数值时,CAP5还没有捕获到此次定时器2的进位!及捕获值差了32678左右!
这个是由于T2PWM输出作为CLOCK提供给timer_4时,时钟输入的同步引起的。所以如果你采用这种方法,就可能会有一个时钟的误差为60M Clock的32768,即为T2PWM的一个脉冲输出。
其实你可以用以下方法来实现同样的功能:
Timer_2的周期设为0xFFFF,并允许CAP和Timer_2的周期中断,在CAP中断中看timer_2中断进入的次数(其为高16位),CAP的计数寄存器为低16位。