This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
使用的是64PIN的28035,我想问一下使用Internal VREG和不使用Internal VREG有啥区别,在什么应用条件下Enable,什么条件下Disable。看了datasheet,还不是很清楚,希望大侠帮忙。
谢谢
Internal VRGE 就是不需要外部的1.8V供电,省了一片3.3V(5V) 转1.8V的LDO或者DC-DC。
用3.3V单电源 供电,不使能VREG
用3.3V和1.8V双电源供电, 使能VREG,将VREGNZ引脚接地,1.8V引脚接2uf以上电容,离引脚越近越好。