This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: C28xx_CPU1: Error: (Error -1137 @ 0x0) Device is held in reset. Take the device out of reset, and retry the operation.

Part Number: TMS320F28379D


1、控制板卡连接不上,debug显示如下错误,示波器采集XRS(F19引脚)获得一个140us的低脉冲,测量3.3V,1.2V电压均正常,且平时XRS为高电平(3.3v)

C28xx_CPU1: Error: (Error -1137 @ 0x0) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 8.1.0.00005)
C28xx_CPU1: Unable to determine target status after 20 attempts
C28xx_CPU1: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging
C28xx_CPU1: Error occurred during flash operation: Could not read 0x0007026D@Data: target is not connected
C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005F444@Data: target is not connected
C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005F444@Data: target is not connected
C28xx_CPU1: Error occurred during flash operation: Could not read 0x00130@Program: target is not connected
C28xx_CPU1: Error executing PLL configuration algorithm. Operation cancelled. (0x0)
C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D200@Data: target is not connected
C28xx_CPU1: File Loader: Memory write failed: Unknown error
C28xx_CPU1: GEL: File: C:\Users\LiuJun\workspace_v9\LAN9252_SPI_379\Debug\LAN9252_SPI_379.out: Load failed.
C28xx_CPU1: Error occurred during flash operation: Could not read register PC: target is not connected
C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005F800@Data: target is not connected
C28xx_CPU1: Error occurred during flash operation: Could not write 0x00000@Program: target is not connected
C28xx_CPU1: Error occurred during flash operation: Cannot enable while the target is disconnected

  • 上边是cc9调试提示错误。

    换做 ccs11,问题变为如下提示

    C28xx_CPU1: Trouble Removing Breakpoint with the Action "Remain Halted" at 0xc0eb: (Error -1066 @ 0xC0EB) Unable to set/clear requested breakpoint. Verify that the breakpoint address is in valid memory. (Emulation package 9.7.0.00213)

    C28xx_CPU1: Error executing PLL configuration algorithm. Operation cancelled. (0x0)

    C28xx_CPU1: File Loader: Memory write failed: Unknown error

    C28xx_CPU1: GEL: File: C:\Users\LiuJun\workspace_v11\LAN9252_SPI_379\Debug\LAN9252_SPI_379.out: Load failed.

    C28xx_CPU1: Trouble Setting Breakpoint with the Action "Remain Halted" at 0xc056: (Error -1066 @ 0xC056) Unable to set/clear requested breakpoint. Verify that the breakpoint address is in valid memory. (Emulation package 9.7.0.00213)

    C28xx_CPU1: Breakpoint Manager: Retrying with a AET breakpoint

  • 你好,第一次出现这种情况吗?你使用的仿真器版本是?

  • 是第一次,新设计的板卡,测试3.3、1.8供电均正常,纹波峰峰值在150mv内;xds100v3 , xml配置测试正常 自己设计的板子 emu0 emu1接4.7k上拉,TRSTN 2.2k下拉,tck频率波形正常 debug时监测到xrs上波形如下图

  • 好的,我向资深工程师咨询后回复您。

  • 你好,抱歉回复晚了。

    连接时XRSn一直是高电平吗?如果它是低电平那么调试探针是不能连接c2000器件的。