This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI的DSP(F28M35)有管脚分配工具吗?

偶尔有些项目需要用TI的DSP,之前用过28335,现在的项目要用F28M35。一直没发现TI有这种工具。
虽然可以手动去分配,但总是担心会出错。
现在很多厂商的DSP MCU ARM什么的都有工具来分配管脚,以防出错。(如ST, INFINEON等)

有的话,请帮忙推荐一下。
谢谢。

  • I already find the tool from TI's website. But I found an issue:

     When I am using the tool, PinMux Utility,  to assign F28M35's PinMux. I found one issue when I assign the EPI port: I want to configure EPI like this: AD0 - AD15, A16-A19, CS0, CS1, WR, RD and ALE. And EPI's other pins, like A20-A23, BSEL0 and BSEL1, I want to use as other functions. (for I just need 20-bit address, and I hold the bsel pins low on chip all the time).

    I think I should select HB/HB16/GP, and then I disable the pins I need not. But once I disable any pin, and then HB/HB16/GP will be unselected. I don't know what it means. Does it mean I can not use these pins I need not as other functions? Or even HB/HB16/GP is unselected, but EPI still can work correctly, and the pins I disable also can be used as other functions?

    Please help to confirm it. thanks!

  • 你好,

    我会把这个问题转到28M35设计团队,但是现在来看,我们都是在程序上手动去设置管脚分配,或者在参考例程上做修改,没有自动生成工具。

  • 你好,

    如果回答满意,请帮忙结掉该贴 :)

  • 我想着是不是等你们把pinmux改好了再结贴呢。呵呵。

  • 好的,我有消息会私密你。