This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28035 : cannot connect to the target

Other Parts Discussed in Thread: CONTROLSUITE

Error connecting to the target:
Error 0x00001200/-1135
Error during: OCS, Target,
Unrecoverable emulation error

控制卡,仿真器供电正常,仿真器连PC机成功,可是一直找不到目标,换F28335试一下,同样出现上面的错误,我怀疑是不是仿真器与控制卡的线路有问题,麻烦给出宝贵建议,谢谢。

  • 您好,建议先检查一下CCS的target configuration file中的配置选项是否正确,再按照板子的quick start guide或者hardware guide的文档检查一下板子的硬件设置是否正确。

  • 看看是否有发现新硬件并成功安装了XDS100v1的驱动,在资源管理器中看看是不是有XDS100的驱动。

    是不是有什么跳线的问题?

  • XDS100v1的驱动已成功安装,资源管理器中有XDS100的驱动,CCS里也显示出XDS100v1连接以及时间,实验板上的跳线是完全按照controlsuite里的要求连得。

  • 可能是跳线的问题,建议您查看相关文档,修改跳线。