CCS 4.2 仿真器 XDS100 V2 出现如下错误
Error connecting to the target: Error 0x80000200/-1041 Fatal Error during: OCS, Device driver: Problem with the Emulation Controller. It is recommended to RESET EMULATOR. This will disconnect each target from the emulator. The targets should then be power cycled or hard reset followed by an emureset and reconnect to each target.
复位仿真器 和板子都不行 Target Configuration 也没有错