This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

f28035的epwm trip zone,按照软件强制中断方式,多长时间进入一次中断?怎么计算呢?



按照Ti中的epwm_trip_zone的例程设置的寄存器的,但是现在程序也能按照我的想法当满足条件时,软件触发中断后,指定的epwm1A强制输出低电平,不满足条件时,按原来情况输出。但是,我现在就是不能计算出多长时间进入一次epwm trip zone的中断?请各位高手指点,谢谢,设置代码如下:

1.在epwm初始化中设置如下:

EALLOW;
EPwm1Regs.TZCTL.bit.TZA = TZ_FORCE_LO;    // Do nothing,no action is taken on EPWMxA
EPwm1Regs.TZCTL.bit.TZB = TZ_NO_CHANGE;          // Force EPWMxB to a low state
EPwm1Regs.TZEINT.bit.OST = 1;     // Enable OST interrupt
EDIS;

2.满足条件时,设置强制触发

   if(Current>= 50)
   {
    EALLOW;
    EPwm2Regs.TZFRC.bit.OST = 1;
       EDIS;
   }
   else
   {

   }

3.epwm trip zone的中断函数

interrupt void EPWM1_TZint_ISR(void)
{
EALLOW;
EPwm1Regs.TZFRC.bit.OST = 0;
EPwm1Regs.TZCLR.bit.OST = 1;
EPwm1Regs.TZCLR.bit.INT = 1;
EDIS;
// Acknowledge this interrupt to receive more interrupts from group 2
PieCtrlRegs.PIEACK.all = PIEACK_GROUP2;
}