This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

在debug F28M35的时候提示无法找到ipc_util.c和sysctl.c等文件

Other Parts Discussed in Thread: CONTROLSUITE

使用你们的Concerto_F28M35xx_control_CARD板子。

然后调试lab1_m3程序。

build project没问题,然后debug,用F6一步一步调试的时候报:

Can't find a source file at "C:/cs30_controlsuite_submodules/cs30_f28m35x_f28m36x/MWare/driverlib/ipc_util.c"

Locate the file or edit the source lookup path to include its location.

 和

Can't find a source file at "C:/cs30_controlsuite_submodules/cs30_f28m35x_f28m36x/MWare/driverlib/sysctl.c"

Locate the file or edit the source lookup path to include its location.

很奇怪,系统为什么会这样提示,我在系统设置的是"${PROJECT_ROOT}/../../MWare"

我的工程目录是放在d:盘下面的,然后MWare放在放在工程目录下。

不知为何系统要在C盘需要MWARE。

在project properties下找了无数次,都找不到C:的这个路径设置在哪,后面没有办法,我就在c盘下创建了C:/cs30_controlsuite_submodules/cs30_f28m35x_f28m36x/MWare这个目录,然后把MWare目录的文件都copy到这目录下。

然后在debug,单步调试,一切正常了。

请问是什么原因啊?

应该在哪里设置WMARE的路径?

谢谢。