This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

我用28069调试时,在FLASH模式下,编译提示一下错误



我用28069调试时,在FLASH模式下,编译提示一下错误:
errors encountered during linking; "Example_2806xAdcSoc.out" not built  ORIGINAL_PROJECT_ROOT line 0 1329273026375 1822

run placement fails for object ".ebss", size 0x8a0 (page 1).  Available ranges: RAML2        size: 0x400        unused: 0x400        max hole: 0x400 .ebss               : > RAML2,      PAGE = 1  ORIGINAL_PROJECT_ROOT line 0 1329273026375 1820

"../F28069.cmd", line 138: error: run placement fails for object ".ebss", size
   0x8a0 (page 1).  Available ranges:
   RAML2        size: 0x400        unused: 0x400        max hole: 0x400    
   .ebss               : > RAML2,      PAGE = 1
warning: entry-point symbol other than "_c_int00" specified:  "code_start"
error: errors encountered during linking; "Example_2806xAdcSoc.out" not built

这个问题要怎么解决?

  • run placement fails for object ".ebss", size 0x8a0 (page 1).  Available ranges: RAML2        size: 0x400        

    这个是说CMD中设定的EBSS的区段只给了0X400的长度,实际需要0X8A0的长度。

    你可以修改CMD文件,把EBSS的区段给大一点。

    比如把:

      RAML2       : origin = 0x008C00, length = 0x000400     /* on-chip RAM block L2 */

      RAML3       : origin = 0x009000, length = 0x001000  /* on-chip RAM block L3 */

    改成:

      RAML2       : origin = 0x008C00, length = 0x001400     /* on-chip RAM block L2 */