This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如果想要监视变量Unit32 pluse_number ,每1ms加1,Graph Properties的设置应该怎么设定?
acquisition buffer size 1
dsp data type 32 bit unsigned interger
index increment 1
Q_value 0
sampling rate HZ 1000
start adress pluse_number
Graph最快只能100ms更新一次,所以你应该看不到你的变量是从1,2,3,4这样加上去的。Buffer size是指存在缓存里用于graph显示的数量,所以需要比较大,比如40,120。
你需要在pluse_number前面加&符号。由于只监视一个变量所以buffer size 为1。既然是每1ms加1,那么下面的time display unit设为MS
10#说Graph最快只能100ms更新一次,1ms加1应该显示不了,是不是只有把这个变量放入DBUFF里,然后显示整个buff里的数值。
是的,如果要看到完整的而不是通过系统插值得到的图像,就需要如10#说的那样用到比较大的buff,把这个变量放入buff里,然后显示整个buff里的数值。