This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280039C: 在TMSf280039平台下如何使用MCAN例程7使用多个ID号发送数据

Part Number: TMS320F280039C

#include "driverlib.h"
#include "device.h"
#include "inc/stw_types.h"
#include "inc/stw_dataTypes.h"

//
// Defines.
//
#define NUM_OF_MSG                      (16U)
#define MCAN_STD_ID_FILTER_NUM          (0U)
#define MCAN_EXT_ID_FILTER_NUM          (0U)
#define MCAN_FIFO_0_NUM                 (0U)
#define MCAN_FIFO_0_ELEM_SIZE           (MCAN_ELEM_SIZE_64BYTES)
#define MCAN_FIFO_1_NUM                 (0U)
#define MCAN_FIFO_1_ELEM_SIZE           (MCAN_ELEM_SIZE_64BYTES)
#define MCAN_RX_BUFF_NUM                (0U)
#define MCAN_RX_BUFF_ELEM_SIZE          (MCAN_ELEM_SIZE_64BYTES)
#define MCAN_TX_BUFF_SIZE               (NUM_OF_MSG)
#define MCAN_TX_BUFF_ELEM_SIZE          (MCAN_ELEM_SIZE_64BYTES)
#define MCAN_TX_EVENT_SIZE              (0U)

//
//  Defining Starting Addresses for Message RAM Sections,
//  (Calculated from Macros based on User defined configuration above)
//
#define MCAN_STD_ID_FILT_START_ADDR     (0x0U)  //0
#define MCAN_EXT_ID_FILT_START_ADDR     (MCAN_STD_ID_FILT_START_ADDR + ((MCAN_STD_ID_FILTER_NUM * MCANSS_STD_ID_FILTER_SIZE_WORDS * 4U)))
#define MCAN_FIFO_0_START_ADDR          (MCAN_EXT_ID_FILT_START_ADDR + ((MCAN_EXT_ID_FILTER_NUM * MCANSS_EXT_ID_FILTER_SIZE_WORDS * 4U)))
#define MCAN_FIFO_1_START_ADDR          (MCAN_FIFO_0_START_ADDR + (MCAN_getMsgObjSize(MCAN_FIFO_0_ELEM_SIZE) * 4U * MCAN_FIFO_0_NUM))
#define MCAN_RX_BUFF_START_ADDR         (MCAN_FIFO_1_START_ADDR + (MCAN_getMsgObjSize(MCAN_FIFO_1_ELEM_SIZE) * 4U * MCAN_FIFO_1_NUM))
#define MCAN_TX_BUFF_START_ADDR         (MCAN_RX_BUFF_START_ADDR + (MCAN_getMsgObjSize(MCAN_RX_BUFF_ELEM_SIZE) * 4U * MCAN_RX_BUFF_NUM))
#define MCAN_TX_EVENT_START_ADDR        (MCAN_TX_BUFF_START_ADDR + (MCAN_getMsgObjSize(MCAN_TX_BUFF_ELEM_SIZE) * 4U * MCAN_TX_BUFF_SIZE))


//
// Global Variables.
//
int32_t     error = 0;
MCAN_TxBufElement txMsg[NUM_OF_MSG];
int32_t loopCnt = 0U;

//
// Function Prototype.
//
static void MCANConfig(void);
int32_t TimeCoun;
int32_t State;
void main()
{
    int i = 0;
    volatile uint32_t mode = 0U;
    uint32_t dataBytes = 8;

    //
    // Initialize device clock and peripherals
    //
    Device_init();

    //
    // Initialize GPIO and configure GPIO pins for CANTX/CANRX
    //
    Device_initGPIO();

    //
    // Configure the divisor for the MCAN bit-clock
    //
    SysCtl_setMCANClk(SYSCTL_MCANCLK_DIV_3);


    //
    // Configuring the GPIOs for MCAN.
    //
    GPIO_setPinConfig(DEVICE_GPIO_CFG_MCANRXA);
    GPIO_setPinConfig(DEVICE_GPIO_CFG_MCANTXA);

    //
    // Initialize message to transmit.
    //
    txMsg[0].id       = ((uint32_t)(0x15A5A5A5)) ;
    txMsg[0].rtr      = 0U;
    txMsg[0].xtd      = 1U;
    txMsg[0].esi      = 0U;
    txMsg[0].dlc      = 8U;
    txMsg[0].brs      = 0U;
    txMsg[0].fdf      = 0U;
    txMsg[0].efc      = 1U;
    txMsg[0].mm       = 0xAAU;
    txMsg[0].data[i]  = 0x1;
    for(i = 1; i < dataBytes; i++)
    {
        txMsg[loopCnt].data[i]  = txMsg[loopCnt].data[i-1] + 1;
    }
//       // Initialize message to transmit.
       txMsg[1].id       = ((uint32_t)(0x15A5A5A6)) ;
       txMsg[1].rtr      = 0U;
       txMsg[1].xtd      = 1U;
       txMsg[1].esi      = 0U;
       txMsg[1].dlc      = 8U;
       txMsg[1].brs      = 0U;
       txMsg[1].fdf      = 0U;
       txMsg[1].efc      = 1U;
       txMsg[1].mm       = 0xAAU;
       txMsg[1].data[i]  = 0x1;
       for(i = 1; i < dataBytes; i++)
       {
           txMsg[1].data[i]  = txMsg[1].data[i-1] + 1;
       }
//       i = 0;
    //
    // Configure the MCAN Module.
    //
    MCANConfig();

    //
    // Write message to Message RAM.
    //

    MCAN_writeMsgRam(MCANA_DRIVER_BASE, MCAN_MEM_TYPE_FIFO, 0,
                         &txMsg[0]);
    MCAN_writeMsgRam(MCANA_DRIVER_BASE, MCAN_MEM_TYPE_FIFO, 1,
                            &txMsg[1]);

    while(1)
    {
        //
        // Add request for all transmission.
        HWREG(MCANA_DRIVER_BASE + MCAN_TXBAR) = 0x00000001;

        //
        // Wait till all the messages are transmitted.
        //
        while(MCAN_getTxBufReqPend(MCANA_DRIVER_BASE))
        {
        }
    }

    //
    // Stop Application.
    //
    asm("   ESTOP0");
}

static void MCANConfig(void)
{
    MCAN_InitParams initParams;
    MCAN_MsgRAMConfigParams    msgRAMConfigParams;
    MCAN_BitTimingParams       bitTimes;

    //
    //  Initializing all structs to zero to prevent stray values
    //
    memset(&initParams, 0, sizeof(initParams));
    memset(&msgRAMConfigParams, 0, sizeof(msgRAMConfigParams));
    memset(&bitTimes, 0, sizeof(bitTimes));

    //
    // Initialize MCAN Init parameters.
    //
    initParams.fdMode            = 0x0U; // FD operation disabled.
    initParams.brsEnable         = 0x0U; // Bit rate switching for
                                         // transmissions disabled.

    //
    // Initialize Message RAM Sections Configuration Parameters
    //
    msgRAMConfigParams.txStartAddr          = MCAN_TX_BUFF_START_ADDR;
    // Tx Buffers Start Address.
    msgRAMConfigParams.txBufNum             = MCAN_TX_BUFF_SIZE;
    // Number of Dedicated Transmit Buffers.
    msgRAMConfigParams.txBufMode            = 0U;
    msgRAMConfigParams.txBufElemSize        = MCAN_TX_BUFF_ELEM_SIZE;
    // Tx Buffer Element Size.

    //
    // Initialize bit timings.
    //
    bitTimes.nomRatePrescalar   = 0x3U; // Nominal Baud Rate Pre-scaler.
    bitTimes.nomTimeSeg1        = 0x9U; // Nominal Time segment before SP.
    bitTimes.nomTimeSeg2        = 0x8U; // Nominal Time segment after SP.
    bitTimes.nomSynchJumpWidth  = 0x8U; // Nominal SJW Range.

    //
    // Wait for memory initialization to happen.
    //
    while(FALSE == MCAN_isMemInitDone(MCANA_DRIVER_BASE))
    {
    }

    //
    // Put MCAN in SW initialization mode.
    //
    MCAN_setOpMode(MCANA_DRIVER_BASE, MCAN_OPERATION_MODE_SW_INIT);

    //
    // Wait till MCAN is not initialized.
    //
    while (MCAN_OPERATION_MODE_SW_INIT != MCAN_getOpMode(MCANA_DRIVER_BASE))
    {}

    //
    // Initialize MCAN module.
    //
    MCAN_init(MCANA_DRIVER_BASE, &initParams);

    //
    // Configure Bit timings.
    //
    MCAN_setBitTime(MCANA_DRIVER_BASE, &bitTimes);

    //
    // Configure Message RAM Sections
    //
    MCAN_msgRAMConfig(MCANA_DRIVER_BASE, &msgRAMConfigParams);

    //
    // Take MCAN out of the SW initialization mode
    //
    MCAN_setOpMode(MCANA_DRIVER_BASE, MCAN_OPERATION_MODE_NORMAL);

    while (MCAN_OPERATION_MODE_NORMAL != MCAN_getOpMode(MCANA_DRIVER_BASE))
    {

    }
}
我修改了这个例程,使用两个ID发数据,但是只有第二个ID  ( 0x15A5A5A6)在发数据,不知道问题出在哪里 ,请求帮助!!!谢谢