This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI-G3 PLC

Other Parts Discussed in Thread: AES-128

请问现在TI在基于G3标准的电力线载波通信的最新方案是什么?

  • wen

    可以在这个网址查找到G3的方案信息:http://www.ti.com.cn/lsds/ti_zh/apps/smartgrid/plcmodem/product.page

    G3 Data Concentrator 
    文档请求
    ERDF specs based PLC modem communication standard designed for Medium and Low Voltage Line for Automatic Meter Management and smart grid applications

    Open, public and non-proprietary telecommunications architecture to enable the building of smart grids. DC = Data Concentrator which manages and maintains the nodes in the network.

    • Low Frequency Narrowband OFDM
    • Cenelec A Band
    • Up to 46 kbps PHY data rate
    • 6LowPAN adaptation to support IPv6
    • AES-128
    • Up to 1024 nodes network
    • point to point, star, mesh network topology
    • Co-exist with IEC61334
    • Crossing transformers
    • Dynamic channel adaptations
    • DC for Automatic Electrical Meters remote reading (AMR)
    • MV-MV WAN connection
    • Controller for Grid-to-home access network
    • LED lighting and Solar inverter control center
    G3 FCC 
    文档请求
    ERDF specs based PLC modem communication standard designed for Medium and Low Voltage Line for Automatic Meter Management and smart grid applications. 
    Implementation based on Concerto™ plus discrete AFE
    • Low Frequency Narrowband OFDM
    • Cenelec A/B/C/D, FCC and ARIB bands
    • up to 141 kbps PHY data rate
    • 6LowPAN adaptation to support IPV6
    • AES-128
    • point to point, star, mesh network topology
    • Co-exist with IEC61334
    • Crossing transformers
    • Dynamic channel adaptations
    • Electrical Meters remote reading
    • Any smart grid application compatible with Cenelec A/B/C/D, FCC, and ARIB frequency Band
    • References