This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
编了一个很简单的程序,程序编译都是正确的,没有任何错误和安全警告。
烧进flash中在线调试,烧写成功之后,点击go main,CCS3.3 messages中报如下错误:
Trouble Setting Breakpoint with the Action "Terminate GEL_Go()" at 0x3f434f: Error 0x00000008/-1066 Error during: Break Point, Cannot set/verify breakpoint at 0x003F434F
Breakpoint Manager: Retrying with a Legacy Hardware breakpoint
感谢您的回复,按你说的设置了一下,按go main后,依然提示:
Trouble Setting Breakpoint with the Action "Terminate GEL_Go()" at 0x3f434f: Error 0x00000008/-1066 Error during: Break Point, Cannot set/verify breakpoint at 0x003F434F
Breakpoint Manager: Retrying with a Legacy Hardware breakpoint
⊙﹏⊙b汗,居然还没有解决。
我没能在我这里重复这种现象。
楼主做下面几件事,再试试。
1、在CCS-->debug-->breakpoints中点remove all。去除所有的breakpoint
2、如上面所说在CCSv3-->option-->Cuctomize-->program/project/CIO中的ProgramLoad 中的1,3,4,5打钩
3、重新编译你的工程,重新烧写FLASH。
4、此时breakpoints显示中没有灰的或者红的breakpoint
然后go main看看能不能正常,如果直接在main函数里面双击设置硬件断点是否能够设置。CCSV3.3是最新的版本吗。
CCSV3.3最新版本下载:
楼主,我也遇到与你描述的相同问题。
重新建立工程后,也按照Forrest提出的4点重新设定。问题还是存在的。
是否是SEED 510plus仿真器的原因?!
使用XDS100 USB简易仿真器就没有该问题。