從controlsuite導入ccs5.2 建立後錯誤如下
errors 9
Description Resource Path Location Type
gmake: *** No rule to make target `D:/ti/ccsv5/eclipse/CONTROLSUITE_F2803x_APPLIB_DRIVERS_ROOT/Util_DLOG4CHC.asm', needed by `Util_DLOG4CHC.obj'. SolarExplorer_PVInverter_F2803x Unknown C/C++ Problem
gmake: *** No rule to make target `D:/ti/ccsv5/eclipse/CONTROLSUITE_F2803x_DEVICE_SUPPORT_ROOT/DSP2803x_common/source/DSP2803x_CodeStartBranch.asm', needed by `DSP2803x_CodeStartBranch.obj'. SolarExplorer_PVInverter_F2803x Unknown C/C++ Problem
gmake: *** No rule to make target `D:/ti/ccsv5/eclipse/CONTROLSUITE_F2803x_DEVICE_SUPPORT_ROOT/DSP2803x_common/source/DSP2803x_usDelay.asm', needed by `DSP2803x_usDelay.obj'. SolarExplorer_PVInverter_F2803x Unknown C/C++ Problem
gmake: *** No rule to make target `D:/ti/ccsv5/eclipse/CONTROLSUITE_F2803x_DEVICE_SUPPORT_ROOT/DSP2803x_headers/cmd/DSP2803x_Headers_nonBIOS.cmd', needed by `SolarExplorer_PVInverter.out'. SolarExplorer_PVInverter_F2803x Unknown C/C++ Problem
gmake: *** No rule to make target `D:/ti/ccsv5/eclipse/CONTROLSUITE_F2803x_DEVICE_SUPPORT_ROOT/DSP2803x_headers/source/DSP2803x_GlobalVariableDefs.c', needed by `DSP2803x_GlobalVariableDefs.obj'. SolarExplorer_PVInverter_F2803x Unknown C/C++ Problem
gmake: *** No rule to make target `D:/ti/ccsv5/eclipse/CONTROLSUITE_F2803x_POWERLIB_ROOT/C/ADC_SOC_Cnf.c', needed by `ADC_SOC_Cnf.obj'. SolarExplorer_PVInverter_F2803x Unknown C/C++ Problem
gmake: *** No rule to make target `D:/ti/ccsv5/eclipse/CONTROLSUITE_F2803x_POWERLIB_ROOT/C/PWM_1ch_UpDwnCntCompl_Cnf.c', needed by `PWM_1ch_UpDwnCntCompl_Cnf.obj'. SolarExplorer_PVInverter_F2803x Unknown C/C++ Problem
gmake: *** No rule to make target `D:/ti/ccsv5/eclipse/CONTROLSUITE_IQMATH_ROOT/lib/IQmath.lib', needed by `SolarExplorer_PVInverter.out'. SolarExplorer_PVInverter_F2803x Unknown C/C++ Problem
gmake: *** No rule to make target `D:/ti/ccsv5/eclipse/CONTROLSUITE_SGENLIB_ROOT/lib/C28x_SGEN_Lib_fixed.lib', needed by `SolarExplorer_PVInverter.out'. SolarExplorer_PVInverter_F2803x Unknown C/C++ Problem
Description Resource Path Location Type
This project contains unresolved buildable linked resources. It might not build as expected. SolarExplorer_PVInverter_F2803x project TI Problem Marker
This project was created using a version of compiler that is not currently installed: 5.2.6 [C2000]. Another version of the compiler will be used during build: 6.1.0. Please install the compiler of the required version, or migrate the project to one of the available compiler versions by adjusting project properties. SolarExplorer_PVInverter_F2803x properties TI Problem Marker