我尝试用spi通讯为两台28335做沟通,但不论怎么发送讯号,从设备就是无法从spirxbuf读取到值,能否有人能给予一段最简单spi沟通编码?
感谢!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我尝试用spi通讯为两台28335做沟通,但不论怎么发送讯号,从设备就是无法从spirxbuf读取到值,能否有人能给予一段最简单spi沟通编码?
感谢!!
也就是说假如是0000 0001这样是8个FIFO 0000 0000 0000 0001这样是16个FIFO吗?
想请问SPISTEA,有办法自行控制是在低电平或者高电平状态吗?
我的意思是能够自己控制让他高电瓶或者低电平吗?
因为我要透过SPI控制别块晶片,因此可能需要能控制ste
我如果把GpioCtrlRegs.GPAMUX2.bit.GPIO19=1改成GpioCtrlRegs.GPAMUX2.bit.GPIO19=00就能让它变成IO管脚对吗?
那在程式中要让他高电位或低电位,那段程式是要如何写?
应该是XXXXXXXXX=1或0,其中的XXXXXXXX要如何写?
GpioCtrlRegs.GPADIR.bit.GPIO19 = 1;关于这段,我是放在程式编译之前,而不是放在SPI.C里面,这样对吗?
SpiaRegs.SPITXBUF=(data<<8); 中DATA<<8的意思是?