This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C2000 Piccolo F28027开发板上电后无输出

        最近使用C2000-launchpad F28027.用usb可以正常烧写程序(包含EPWM和ADC),引脚输出正常。断开USB直接用5v直流稳压给开发板供电时,pwm引脚没有输出。开发板上的TX和RX led也点亮了,但实际上我的程序里并没有用到这个模块的功能。不知道是什么原因。我试讲程序写进flash的,也测过这种情况下开发板的5V和3.3V引脚都是正常的。请高人指点!!多谢啦~

  • 电源如果真的没问题的话,主要差别在仿真器那边。

    因为如果楼主用的USB供电,USB除了有5V供电的功能以外,还具有仿真器XDS100的功能。

    所以楼主的程序应该是在RAM中运行的? 烧写到Flash中了么?

    开发板最下面的4个LED,GPIO0~3很容易受到外面的静电影响,比如你拿手随便触碰两侧的针脚,LED就会闪烁,因此TX LED和RX LED的亮灭可以忽略。

    我觉得还是程序的问题,或者看看有个跳线BOOT选择的薄码开关,是否薄码正确,应该都在上方。