This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C2000 28035 EPWM 配置的问题 20140518



各位好,我想请教一个问题:

首先,我知道在28035的EPWM配置中,通过配置寄存器TBPHS,可以让不同的EPWM模块之间,在各自的TBCTR载波上,产生一个相位差;

比如:EPWM1和EPWM2 的TBPRD都为3000,都为UP-DOWN计数模式;

          那么如果EPWM2模块的TBPHS=3000,PHSDIR =0(向下开始计数),

          则由于EPWM2模块的TBCTR载波要滞后于EPWM1模块半个周期,所以EPWM2整个模块要滞后于EPWM1模块;

         若采用完全同样的比较值翻转方式,则EPWM2A要滞后于EPWM1A半个周期,EPWM2B也要滞后于EPWM1B半个周期。

那么,上面是两个不同EPWM模块之间的相位差;

 

我的问题是:

在同一个EPWM模块中(就拿EPWM1模块来说),它自己的2个EPWM1A、EPWM1B之间,能不能也通过寄存器,配置成     EPWM1B的载波    一直滞后EPWM1A的载波    半个周期?   

(效果同上面的不同EPWM模块之间的相位差“类似”,只不过这次的相位差是同一个EPWM模块内部的,2个不同 EPWMxA、EPWMxB 端口之间的延时)

能不能实现?

能实现的话,是配置哪个寄存器的值?

能否直接提供代码?(EPWMxB 的TBCTR载波     滞后于      EPWMxA的TBCTR载波    半个载波周期