void F281X_EV1_PWM_Update(PWMGEN *p)
{
int16 MPeriod;
int32 Tmp;
// Compute the timer period (Q0) from the period modulation input (Q15)
Tmp = (int32)p->PeriodMax*(int32)p->MfuncPeriod; // Q15 = Q0*Q15
MPeriod = (int16)(Tmp>>16) + (int16)(p->PeriodMax>>1); // Q0 = (Q15->Q0)/2 + (Q0/2)
EvaRegs.T1PR = MPeriod;
// Compute the compare 1 (Q0) from the PWM 1&2 duty cycle ratio (Q15)
Tmp = (int32)MPeriod*(int32)p->MfuncC1; // Q15 = Q0*Q15
EvaRegs.CMPR1 = (int16)(Tmp>>16) + (int16)(MPeriod>>1); // Q0 = (Q15->Q0)/2 + (Q0/2)
// Compute the compare 2 (Q0) from the PWM 3&4 duty cycle ratio (Q15)
Tmp = (int32)MPeriod*(int32)p->MfuncC2; // Q15 = Q0*Q15
EvaRegs.CMPR2 = (int16)(Tmp>>16) + (int16)(MPeriod>>1); // Q0 = (Q15->Q0)/2 + (Q0/2)
// Compute the compare 3 (Q0) from the PWM 5&6 duty cycle ratio (Q15)
Tmp = (int32)MPeriod*(int32)p->MfuncC3; // Q15 = Q0*Q15
EvaRegs.CMPR3 = (int16)(Tmp>>16) + (int16)(MPeriod>>1); // Q0 = (Q15->Q0)/2 + (Q0/2)
}
请问,EvaRegs.T1PR问什么要重新计算?计算原理是什么,还有MfuncPeriod的初值是0X7FFF,这个又是什么作用?CMPR的值的计算原理是什么呢?谢谢