This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

永磁同步电机驱动中电流环的问题

本人基于F2812用TI提供的永磁同步电机FOC控制的代码去做永磁同步直线电机驱动,开环验证没问题(Ud=0,Uq=0.15),电机正常运行,但是电流环实验中遇到问题:

在PI参数整定后,用示波器观察id,iq都能很好跟随给定,但iq需设定很大电流(id=0,iq=0.5以上,标幺最大值为11.25A,)电机才能运行起来,否则在原位置抖动(频率不大),有向前运行的趋势,但无法前行。

有没有哪位朋友遇到同样问题的,恳请支招!!!万分感谢啊!!!!!

ps:电机额定电流为4.4A,峰值电流为11.3A。