This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于dsp程序中的数据类型



各位高工:

       你们好!最近写了个PI程序,其中qKp是比例系数,用了Q6格式;qKi是积分参数,用Q14格式,参数全部设置成长整形int32,给定一个小小的正误差,理论上不应该饱和,但是程序运行却出现了负饱和,很明显是错误的,我想是不是DSP中不能用long*long型,还是移位时出现什么问题,想请帮个忙,看看简单的程序,程序如下:

定义了全局变量

static int32 qKp=2500;  //PI调节的比例系数   Q6格式
static int32 qKi=20;    //PI调节的积分系数   Q14格式
static int32 qsum=0;       //PI调节的积分项
static int32 qsummax=2949120; //积分项正饱和值
static int32 qsummin=-2949120;//积分项负饱和值
static int32 qresult=0;       //PI调节输出结果
static int32 spd_max= 480;    //PI正饱和值
static int32 spd_min=-480;    //PI负饱和值PI程序:

void PI()
{
 int32 lgtmpi,lgtmpp,spd_err;             //spd_err是给定值与实际值的误差,lgtmpi,lgtmpp是临时变量

 spd_err=10-real_spd;                    //real_spd是实际值

 qsum=qsum+qKi*spd_err;                  //积分项
 if(qsum>=qsummax) qsum=qsummax;
 else if(qsum<=qsummin) qsum=qsummin;     //积分饱和处理
 lgtmpi=qsum>>14;

 lgtmpp=qKp*spd_err>>6;
 qresult=lgtmpi+lgtmpp;                  //PI公式计算

 if(qresult>=spd_max)      {qresult=spd_max;}
 else if(qresult<=spd_min) {qresult=spd_min;}   //pi饱和处理
}

实验中是令real_spd=0;但是观测的结果是pi出现负饱和,真的不知道DSP内部定点运算是怎么算的,希望能请教到您!谢谢!