This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28027脱机运行问题



F28027,CCS3.3,仿真时正常,有窗口数据打印输出,脱机时选用28027.cmd,调用了

MemCopy(&RamfuncsLoadStart, &RamfuncsLoadEnd, &RamfuncsRunStart);  

InitFlash();

但就是串口没数据输出,不知道哪个地方的问题,求解???????

  • Mak he,

    你这里有可能是程序Flash搬到Ram中没用好,你试试不搬程序脱机测试串口通信有问题吗?

  • Joey Mao,

           我不将Flash搬到Ram也有问题,我的cmd文件如下,不知道那个地方有问题?另外,我脱机时用JTAG口将程序烧写到Flash后,用的是28027.cmd,不断开连接,单步执行也可以,这还是处于仿真状态吗?

    MEMORY
    {
    PAGE 0:    /* Program Memory */
               /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE1 for data allocation */

       PRAML0      : origin = 0x008000, length = 0x000800     /* on-chip RAM block L0 */
       OTP         : origin = 0x3D7800, length = 0x000400     /* on-chip OTP */
       FLASHD      : origin = 0x3F0000, length = 0x002000     /* on-chip FLASH */
       FLASHC      : origin = 0x3F2000, length = 0x002000     /* on-chip FLASH */
       FLASHA      : origin = 0x3F6000, length = 0x001F80     /* on-chip FLASH */
       CSM_RSVD    : origin = 0x3F7F80, length = 0x000076     /* Part of FLASHA.  Program with all 0x0000 when CSM is in use. */
       BEGIN       : origin = 0x3F7FF6, length = 0x000002     /* Part of FLASHA.  Used for "boot to Flash" bootloader mode. */
       CSM_PWL_P0  : origin = 0x3F7FF8, length = 0x000008     /* Part of FLASHA.  CSM password locations in FLASHA */

       IQTABLES    : origin = 0x3FE000, length = 0x000B50     /* IQ Math Tables in Boot ROM */
       IQTABLES2   : origin = 0x3FEB50, length = 0x00008C     /* IQ Math Tables in Boot ROM */
       IQTABLES3   : origin = 0x3FEBDC, length = 0x0000AA   /* IQ Math Tables in Boot ROM */

       ROM         : origin = 0x3FF27C, length = 0x000D44     /* Boot ROM */
       RESET       : origin = 0x3FFFC0, length = 0x000002     /* part of boot ROM  */
       VECTORS     : origin = 0x3FFFC2, length = 0x00003E     /* part of boot ROM  */

    PAGE 1 :   /* Data Memory */
               /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE0 for program allocation */
               /* Registers remain on PAGE1                                                  */

       BOOT_RSVD   : origin = 0x000000, length = 0x000050     /* Part of M0, BOOT rom will use this for stack */
       RAMM0       : origin = 0x000050, length = 0x0003B0     /* on-chip RAM block M0 */
       RAMM1       : origin = 0x000400, length = 0x000400     /* on-chip RAM block M1 */
       DRAML0      : origin = 0x008800, length = 0x000800     /* on-chip RAM block L0 */
       FLASHB      : origin = 0x3F4000, length = 0x002000     /* on-chip FLASH */
    }

    SECTIONS
    {

       /* Allocate program areas: */
       .cinit              : > FLASHA       PAGE = 0
       .pinit              : > FLASHA,      PAGE = 0
       .text               : > FLASHA       PAGE = 0
       codestart           : > BEGIN        PAGE = 0
      /* ramfuncs      : > FLASHA       PAGE = 0 /*modfi at 20140528*//*不搬运使用,不搬运时将MemCopy()屏蔽*/
       
       ramfuncs            : LOAD = FLASHA,
                             RUN = PRAML0,
                             LOAD_START(_RamfuncsLoadStart),
                             LOAD_END(_RamfuncsLoadEnd),
                             RUN_START(_RamfuncsRunStart),
                             PAGE = 0 /*搬运时使用,将MemCopy()放开*/

       csmpasswds          : > CSM_PWL_P0   PAGE = 0
       csm_rsvd            : > CSM_RSVD     PAGE = 0

       /* Allocate uninitalized data sections: */
       .stack              : > RAMM0        PAGE = 1
       .ebss               : > DRAML0       PAGE = 1
       .esysmem            : > DRAML0       PAGE = 1

       /* Initalized sections go in Flash */
       /* For SDFlash to program these, they must be allocated to page 0 */
       .econst             : > FLASHA       PAGE = 0
       .switch             : > FLASHA       PAGE = 0

       /* Allocate IQ math areas: */
       IQmath              : > FLASHA       PAGE = 0            /* Math Code */
       IQmathTables        : > IQTABLES,    PAGE = 0, TYPE = NOLOAD

       /* Uncomment the section below if calling the IQNexp() or IQexp()
          functions from the IQMath.lib library in order to utilize the
          relevant IQ Math table in Boot ROM (This saves space and Boot ROM
          is 1 wait-state). If this section is not uncommented, IQmathTables2
          will be loaded into other memory (SARAM, Flash, etc.) and will take
          up space, but 0 wait-state is possible.
       */
       /*
       IQmathTables2    : > IQTABLES2, PAGE = 0, TYPE = NOLOAD
       {

                  IQmath.lib<IQNexpTable.obj> (IQmathTablesRam)

       }
       */
       /* Uncomment the section below if calling the IQNasin() or IQasin()
          functions from the IQMath.lib library in order to utilize the
          relevant IQ Math table in Boot ROM (This saves space and Boot ROM
          is 1 wait-state). If this section is not uncommented, IQmathTables2
          will be loaded into other memory (SARAM, Flash, etc.) and will take
          up space, but 0 wait-state is possible.
       */
       /*
       IQmathTables3    : > IQTABLES3, PAGE = 0, TYPE = NOLOAD
       {

                  IQmath.lib<IQNasinTable.obj> (IQmathTablesRam)

       }
       */

       /* .reset is a standard section used by the compiler.  It contains the */
       /* the address of the start of _c_int00 for C Code.   /*
       /* When using the boot ROM this section and the CPU vector */
       /* table is not needed.  Thus the default type is set here to  */
       /* DSECT  */
       .reset              : > RESET,      PAGE = 0, TYPE = DSECT
       vectors             : > VECTORS     PAGE = 0, TYPE = DSECT

    }

  • Mak he,

    你所说的这句话我有两点疑问:我脱机时用JTAG口将程序烧写到Flash后,用的是28027.cmd,��断开连接,单步执行也可以,这还是处于仿真状态吗?

    1、什么叫脱机用JTAG口烧程序?

    2、断开连接,单步执行:是指断开仿真器吗?那你如何单步执行的?用CCS操作程序执行都不叫脱机运行