This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于TMS320F28xx如何在HP3070上实现在线烧录



我们想用的方法是:直接编写library 测试文件,通过DSP的JTAG端口去download source code,请问这种方法是否可行?如果不可以,请问还有其他什么方法?另外,我们拿到源文件是.S28文件,需要去转换成SVF的格式,TI是否有这样的工具可以转?

  • 楼主,我没有接触过HP3070,但我想这并不妨碍我们进行讨论。

    C2000芯片有2种常用的烧写方法,一种是通过JTAG口,一种是通过串口bootload;2种方法都可行。

    .s28文件里面应该是一些汇编源代码。TI没有工具可以把文件转成SVF格式,但是有HEX2000工具可以把通过CCS编译后生成的.OUT文件转成ASCII-Hex,binary,Intel等格式,如果你有工具可以考虑再转一下。

    关于HEX2000,可以参考下面的文档:

    http://www.ti.com/litv/pdf/spru513d

     

    hex2000.zip
  • 谢谢啦!.S28是MOTO格式的源代码,是的,已问过TI的工程师,HEX2000不能直接转换,可能需要考虑转两次了。