This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
着试我官网下载的cmd文件后修改的
MEMORY { PAGE 0: /* Program Memory */ /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE1 for data allocation */ ZONE0 : origin = 0x002000, length = 0x002000 /* XINTF zone 0 */ ZONE1 : origin = 0x004000, length = 0x002000 /* XINTF zone 1 */ RAML0 : origin = 0x008000, length = 0x001000 /* on-chip RAM block L0 */ ZONE2 : origin = 0x080000, length = 0x080000 /* XINTF zone 2 */ ZONE6 : origin = 0x100000, length = 0x080000 /* XINTF zone 6 */ OTP : origin = 0x3D7800, length = 0x000800 /* on-chip OTP */ FLASHJ : origin = 0x3D8000, length = 0x002000 /* on-chip FLASH */ FLASHI : origin = 0x3DA000, length = 0x002000 /* on-chip FLASH */ FLASHH : origin = 0x3DC000, length = 0x004000 /* on-chip FLASH */ FLASHG : origin = 0x3E0000, length = 0x004000 /* on-chip FLASH */ FLASHF : origin = 0x3E4000, length = 0x004000 /* on-chip FLASH */ FLASHE : origin = 0x3E8000, length = 0x004000 /* on-chip FLASH */ FLASHD : origin = 0x3EC000, length = 0x004000 /* on-chip FLASH */ FLASHC : origin = 0x3F0000, length = 0x004000 /* on-chip FLASH */ FLASHA : origin = 0x3F6000, length = 0x001F80 /* on-chip FLASH */ CSM_RSVD : origin = 0x3F7F80, length = 0x000076 /* Part of FLASHA. Program with all 0x0000 when CSM is in use. */ BEGIN : origin = 0x3F7FF6, length = 0x000002 /* Part of FLASHA. Used for "boot to Flash" bootloader mode. */ CSM_PWL : origin = 0x3F7FF8, length = 0x000008 /* Part of FLASHA. CSM password locations in FLASHA */ /* ZONE7 : origin = 0x3FC000, length = 0x003FC0 /* XINTF zone 7 available if MP/MCn=1 */ ROM : origin = 0x3FF000, length = 0x000FC0 /* Boot ROM available if MP/MCn=0 */ RESET : origin = 0x3FFFC0, length = 0x000002 /* part of boot ROM (MP/MCn=0) or XINTF zone 7 (MP/MCn=1) */ VECTORS : origin = 0x3FFFC2, length = 0x00003E /* part of boot ROM (MP/MCn=0) or XINTF zone 7 (MP/MCn=1) */ PAGE 1 : /* Data Memory */ /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE0 for program allocation */ /* Registers remain on PAGE1 */ RAMM0 : origin = 0x000000, length = 0x000400 /* on-chip RAM block M0 */ RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */ RAML1 : origin = 0x009000, length = 0x001000 /* on-chip RAM block L1 */ FLASHB : origin = 0x3F4000, length = 0x002000 /* on-chip FLASH */ RAMH0 : origin = 0x3F8000, length = 0x002000 /* on-chip RAM block H0 */ ZONE2tf : origin = 0x084000, length = 0x001FFF } /* Allocate sections to memory blocks. Note: codestart user defined section in DSP28_CodeStartBranch.asm used to redirect code execution when booting to flash ramfuncs user defined section to store functions that will be copied from Flash into RAM */ SECTIONS { /* Allocate program areas: */ .cinit : > FLASHA PAGE = 0 .pinit : > FLASHA, PAGE = 0 .text : > FLASHA PAGE = 0 codestart : > BEGIN PAGE = 0 ramfuncs : LOAD = FLASHD, RUN = RAML0, LOAD_START(_RamfuncsLoadStart), LOAD_END(_RamfuncsLoadEnd), RUN_START(_RamfuncsRunStart), PAGE = 0 csmpasswds : > CSM_PWL PAGE = 0 csm_rsvd : > CSM_RSVD PAGE = 0 /* Allocate uninitalized data sections: */ .stack : > RAMM0 PAGE = 1 .ebss : > RAML1 PAGE = 1 .esysmem : > RAMH0 PAGE = 1 /* Initalized sections go in Flash */ /* For SDFlash to program these, they must be allocated to page 0 */ .econst : > FLASHA PAGE = 0 .switch : > FLASHA PAGE = 0 /* Allocate IQ math areas: */ IQmath : > FLASHC PAGE = 0 /* Math Code */ IQmathTables : > ROM PAGE = 0, TYPE = NOLOAD /* Math Tables In ROM */ /* .reset is a standard section used by the compiler. It contains the */ /* the address of the start of _c_int00 for C Code. /* /* When using the boot ROM this section and the CPU vector */ /* table is not needed. Thus the default type is set here to */ /* DSECT */ .reset : > RESET, PAGE = 0, TYPE = DSECT vectors : > VECTORS PAGE = 0, TYPE = DSECT FFTipcb3 ALIGN(256) : {} > RAMH0 PAGE=1 FFTipcb4 ALIGN(256) : {} > RAMH0 PAGE=1 FFTmag : > RAMH0 PAGE=1 FFTtf : > RAML0 PAGE=0 }
烧写的时候出现错误
Warning: This program contains initialized RAM data.
It may run successfully under Code Composer Studio
but not as a standalone system because of this. If
your Flash program requires initialized data in RAM,
you will need to write Flash code to initialize RAM memory.
Erase/Program/Verify Operation succeeded
**** End Erase/Program/Verify Operation. ***
感觉还是CMD没配置对,串口等其他部分都能运行
我试着放到FLASH里过
FFTipcb3 ALIGN(256) : {} > FLASHC PAGE = 0
FFTipcb4 ALIGN(256) : {} > FLASHC PAGE = 0
FFTmag : > FLASHC PAGE = 0
FFTtf : > FLASHC PAGE = 0
还是不运行