This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F2812下载程序时出现地址验证失败问题(Data verification failed at address 0x8576...)

下载程序时遇到一个问题,请求指教!问题描述如下:
使用芯片:F2812
仿真器:XDS100USB
开发环境:CCS3.3


打开板子电源,复位引脚电压为2.4V,当连接好仿真器打开CCS3.3并与板子连接后,复位引脚电压变为3.2V。

下载程序,单步运行到主函数,然后再单步就会出现问题:“Trouble Removing Breakpoint with the Action "Continue or Finish Stepping" at 0x8504: Error 0x00000008/-1066 Error during: Break Point, Cannot set/verify breakpoint at 0x00008504”。

然后用Debug->Reset CPU,再次下载程序时会提示:“Data verification failed at address 0x8576.Please verify target memory and memory map.”

开始我以为我配置的CMD文件有问题,但是0x8576确实是在L0 SARAM(0x008000-0x009000)段中,所以这段RAM应该是可以用的。

CMD文件配置如下所示:

MEMORY
{
PAGE 0 :
RAML0 : origin = 0x008000, length = 0x001000

PAGE 1 :
/* SARAM */
RAMM0 : origin = 0x000040, length = 0x0003C0
RAMM1 : origin = 0x000400, length = 0x000400
RAMH0 : origin = 0x3f8000, length = 0x002000
}

SECTIONS

{
/* Allocate program areas: */
.reset : > RAML0, PAGE = 0
.text : > RAML0, PAGE = 0
.cinit : > RAML0, PAGE = 0

/* Allocate data areas: */
.stack : > RAMM1, PAGE = 1
.bss : > RAMH0, PAGE = 1
.ebss : > RAMH0, PAGE = 1
.const : > RAMH0, PAGE = 1
.econst : > RAMH0, PAGE = 1
.sysmem : > RAMH0, PAGE = 1
}

我也使用了官方的CMD文件,不过和这个基本差不多,仍然是一样的。

现在出现了这个不能下载的问题不知道如何解决,请求各位有经验人士指导,非常感谢!!