最近想上手FOC,本来想借一个launch pad跑跑TI的示例程序,但看到DMC库里面的例程只支持2803x和2833x,launch pad上的是28027
所以想问一下28027能用DMC库里面的例程么?
另外TI还建议使用DMC legacy么?还是尽量使用controlsuite里面的DMC(但不支持2812啊)?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
最近想上手FOC,本来想借一个launch pad跑跑TI的示例程序,但看到DMC库里面的例程只支持2803x和2833x,launch pad上的是28027
所以想问一下28027能用DMC库里面的例程么?
另外TI还建议使用DMC legacy么?还是尽量使用controlsuite里面的DMC(但不支持2812啊)?
我指的是这些工程
Table 4. Projects in controlSUITE and Legacy
| Motor Type | Description | Legacy | controlSUITE |
| 3-ph ACI | Sensored – Tacho i/p Scalar Control / SVPWM | 281x 280x | 2803x |
| 3-ph ACI | Sensored – Tacho or Encoder Field Oriented Control / SVPWM | 281x 280x | 2803x |
| 3-ph ACI | Sensorless – Direct Flux Estimator Field Oriented Control / SVPWM | 281x 280x | 2803x 2833x |
| 3-ph PMSM | Sensored – Incremental Encoder Field Oriented Control / SVPWM | 281x 280x | 2803x |
| 3-ph PMSM | Sensorless – Sliding Mode Observer Field Oriented Control / SVPWM | 281x 280x | 2803x 2833x |
| 3-ph PMSM | Sensored – Incremental Encoder Position Control / SVPWM | 281x 280x | 2803x |
| 3-ph PMSM | Sensored – Resolver Field Oriented Control / SVPWM | 281x 280x | TBD |
| 3-ph BLDC | Sensored – Hall Effect Sensors Trapezoidal Control | 281x 280x | 2803x |
| 3-ph BLDC | Sensorless – BEMF Sensing Trapezoidal Control | 281x 280x | 2803x |
| 3-ph BLDC | Sensorless – Sinusoidal Control Field Oriented Control / SVPWM | - | 2803x |
| Brushed DC | Sensored – QEP Position and speed control | 281x 280x | Q410 |
| Stepper Motor | Sensorless – Discrete Angle Est. Position and Speed Control | 280x | Q410 |