This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我用ccs5,4导入ccs3.3的文件,编译后出现 gmake: Nothing to be done for `all'.是什么意思
http://e2e.ti.com/support/development_tools/code_composer_studio/f/81/t/215561.aspx
可以参考一下这个解答。
**** Build of configuration Debug for project dsp ****
"C:\\ti\\ccsv6\\utils\\bin\\gmake" -k all
gmake: Nothing to be done for `all'.
**** Build Finished ****
我用CCS6往2812烧flash程序,程序运行不起来,之前的工程是从3.3导入到6里面的,在ram上可以调试,烧到flash就不可以,是为什么呀?
编译没问题,烧写就有上面的提示
谢谢回答
这种问题,要右键工程,选择rebuild project, 然后观察console中的报错信息。
建议可以直接导入一个CCS6的例程,如f28035 flash的例程,C:\ti\controlSUITE\device_support\f2803x\v130\DSP2803x_examples_ccsv5\flash_f28035
然后将例程中一些无关的源文件删掉,复制自己的CCS3.3的源文件进工程,再右键工程,属性,C2000 compiler中设置好头文件包含路径。
再编译。
ERIC