程序如下所示,请问这个程序是什么时候产生中断的,怎么从main的空循环里跳出到中断服务子程序的,谢谢?
//###########################################################################
//
//! \addtogroup f2803x_example_list
//! <h1>SPI Digital Loop Back with Interrupts(spi_loopback_interrupts)</h1>
//!
//! This program uses the internal loop back test mode of the peripheral.
//! Other then boot mode pin configuration, no other hardware configuration
//! is required. Both interrupts and the SPI FIFOs are used.
//!
//! A stream of data is sent and then compared to the received stream.
//! The sent data looks like this: \n
//! 0000 0001 \n
//! 0001 0002 \n
//! 0002 0003 \n
//! .... \n
//! FFFE FFFF \n
//! FFFF 0000 \n
//! etc.. \n
//! This pattern is repeated forever.
//!
//! \b Watch \b Variables \n
//! - \b sdata , Data to send
//! - \b rdata , Received data
//! - \b rdata_point , Used to keep track of the last position in
//! the receive stream for error checking
//
//###########################################################################
// $TI Release: F2803x C/C++ Header Files and Peripheral Examples V127 $
// $Release Date: March 30, 2013 $
//###########################################################################
#include "DSP28x_Project.h" // Device Headerfile and Examples Include File
// Prototype statements for functions found within this file.
// interrupt void ISRTimer2(void);
__interrupt void spiTxFifoIsr(void);
__interrupt void spiRxFifoIsr(void);
void delay_loop(void);
void spi_fifo_init(void);
void error();
Uint16 sdata[2]; // Send data buffer
Uint16 rdata[2]; // Receive data buffer
Uint16 rdata_point; // Keep track of where we are
// in the data stream to check received data
void main(void)
{
Uint16 i;
// Step 1. Initialize System Control:
// PLL, WatchDog, enable Peripheral Clocks
// This example function is found in the DSP2803x_SysCtrl.c file.
InitSysCtrl();
// Step 2. Initalize GPIO:
// This example function is found in the DSP2803x_Gpio.c file and
// illustrates how to set the GPIO to it's default state.
// InitGpio(); // Skipped for this example
// Setup only the GP I/O only for SPI-A functionality
InitSpiaGpio();
// Step 3. Initialize PIE vector table:
// Disable and clear all CPU interrupts
DINT;
IER = 0x0000;
IFR = 0x0000;
// Initialize PIE control registers to their default state:
// This function is found in the DSP2803x_PieCtrl.c file.
InitPieCtrl();
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
// This will populate the entire table, even if the interrupt
// is not used in this example. This is useful for debug purposes.
// The shell ISR routines are found in DSP2803x_DefaultIsr.c.
// This function is found in DSP2803x_PieVect.c.
InitPieVectTable();
// Interrupts that are used in this example are re-mapped to
// ISR functions found within this file.
EALLOW; // This is needed to write to EALLOW protected registers
PieVectTable.SPIRXINTA = &spiRxFifoIsr;
PieVectTable.SPITXINTA = &spiTxFifoIsr;
EDIS; // This is needed to disable write to EALLOW protected registers
// Step 4. Initialize all the Device Peripherals:
// This function is found in DSP2803x_InitPeripherals.c
// InitPeripherals(); // Not required for this example
spi_fifo_init(); // Initialize the SPI only
// Step 5. User specific code, enable interrupts:
// Initalize the send data buffer
for(i=0; i<2; i++)
{
sdata[i] = i;
}
rdata_point = 0;
// Enable interrupts required for this example
PieCtrlRegs.PIECTRL.bit.ENPIE = 1; // Enable the PIE block
PieCtrlRegs.PIEIER6.bit.INTx1=1; // Enable PIE Group 6, INT 1
PieCtrlRegs.PIEIER6.bit.INTx2=1; // Enable PIE Group 6, INT 2
IER=0x20; // Enable CPU INT6
EINT; // Enable Global Interrupts
// Step 6. IDLE loop. Just sit and loop forever (optional):
for(;;);
}
// Some Useful local functions
void delay_loop()
{
long i;
for (i = 0; i < 1000000; i++) {}
}
void error(void)
{
__asm(" ESTOP0"); //Test failed!! Stop!
for (;;);
}
void spi_fifo_init()
{
// Initialize SPI FIFO registers
SpiaRegs.***.bit.SPISWRESET=0; // Reset SPI
SpiaRegs.***.all=0x001F; //16-bit character, Loopback mode
SpiaRegs.***.all=0x0017; //Interrupt enabled, Master/Slave XMIT enabled
SpiaRegs.SPISTS.all=0x0000;
SpiaRegs.SPIBRR=0x0063; // Baud rate
SpiaRegs.SPIFFTX.all=0xC022; // Enable FIFO's, set TX FIFO level to 2 1100 0000 0010 0010
SpiaRegs.SPIFFRX.all=0x0022; // Set RX FIFO level to 2
SpiaRegs.SPIFFCT.all=0x00;
SpiaRegs.SPIPRI.all=0x0010;
SpiaRegs.***.bit.SPISWRESET=1; // Enable SPI
SpiaRegs.SPIFFTX.bit.TXFIFO=1;
SpiaRegs.SPIFFRX.bit.RXFIFORESET=1;
}
__interrupt void spiTxFifoIsr(void)
{
Uint16 i;
for(i=0;i<2;i++)
{
SpiaRegs.SPITXBUF=sdata[i]; // Send data
}
//
// Increment data buffer contents by 1 for
// the next transmit cycle
//
for(i=0;i<2;i++)
{
sdata[i] = sdata[i] + 1;
}
SpiaRegs.SPIFFTX.bit.TXFFINTCLR=1; // Clear Interrupt flag
PieCtrlRegs.PIEACK.all|=0x20; // Issue PIE ACK
}
__interrupt void spiRxFifoIsr(void)
{
Uint16 i;
for(i=0;i<2;i++)
{
rdata[i]=SpiaRegs.SPIRXBUF; // Read data
}
for(i=0;i<2;i++) // Check received data
{
if(rdata[i] != rdata_point+i) error();
}
rdata_point++;
SpiaRegs.SPIFFRX.bit.RXFFOVFCLR=1; // Clear Overflow flag
SpiaRegs.SPIFFRX.bit.RXFFINTCLR=1; // Clear Interrupt flag
PieCtrlRegs.PIEACK.all|=0x20; // Issue PIE ack
}
//===========================================================================
// No more.
//===========================================================================