This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我在ti网站上下载了28035的例程,通过仿真器能够运行里边的ram程序,能够正常调试。也可以通过仿真将flash程序下载片子内,但是flash程序不能调试运行,总感觉一直在bootrom里边运行跳不来,我应用的是ccs3.3.但是用ccs5无论ram还是falsh都可以正常运行,这是为什么?只是ccs的区别吗
在ccs3.3中ram可以正常运行,源程序导入没有错误啊,我直接从ti网站上下载的,除非ti例程错了,问题还是出在设置上,板子上或者ccs3.3设置,具体哪我也不知道,再次请教!
Write EMU_KEY to 0xD00 and EMU_BMODE to 0xD01 via the debugger according to the Boot Mode Table above.这是例程中的原文,请教一下,这句话是什么意思,debugger是指什么在哪里找到?
检查一下工程中是否有CodeStartBranch.asm的源文件,硬件上板子的boot mode是否被改变,是否为flash boot mode。如果是例程错了,你就不可能在CCSV5下成功运行。