This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSP供电模块



用一个LM2940将12V电源稳压到5V,然后使用TPS767d301输出3.3V和1.9V给F28335供电。

 各点输出电压正常,板子与仿真器链接正常,可是在Debug点连续运行时DSP直接不工作(各点电压正常),各个芯片不热。

然后去掉LM2940,用一片L7805CV(1.5A的最大输出电流)给TPS767d301供5V电压,在Debug点连续运行F28335可工作,不过TPS767d301很热,手不敢放到芯片的那种温度。

请问LM2940(1A)不能满足要求吗,是输出电流太小吗?