This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

时钟漂移



各位专家同僚,DSP F2812时钟10s稳定漂移1ms的问题,主要存在以下两个现象:

1、换了好几块晶振,故障现象稳定复现,F2812时钟10s计时快1ms,这是什么原因呢?该怎么解决呢?

2、拆掉晶振,用外部信号发生器模拟晶振,晶振频率30MHz,信号发生器只能发送15MHz的频率,倍频不变,DSP系统时钟由150MHz变为75MHz,重新测试DSP时钟漂移问题,很奇怪的是,TIM寄存器计数值经换算后跟DSP定时器输出值差异很大,这是什么原因呢?还需要更改其他什么配置吗?

感谢各位大神不吝赐教!