This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The relevent schematic is as follow : when i load code with ccs ,it present follow question. And the 'MCU_XRSN' signal waveform as follow
C28xx_CPU1: GEL Output:
Memory Map Initialization Complete
C28xx_CPU1: If erase/program (E/P) operation is being done on one core, the other core should not execute from shared-RAM (SR) as they are used for the E/P code. Also, CPU1 will be halted to determine SR ownership for the CPU which will run the Flash Plugin code, after which CPU1 will be set to run its application. User code execution from SR could commence after both flash banks are programmed.
C28xx_CPU1: Error: (Error -1137 @ 0x0) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 8.1.0.00005)
C28xx_CPU1: Unable to determine target status after 20 attempts
C28xx_CPU1: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging
C28xx_CPU1: Error occurred during flash operation: Could not read 0x0007026D@Data: target is not connected
C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005F444@Data: target is not connected
C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005F444@Data: target is not connected
C28xx_CPU1: Error occurred during flash operation: Could not read 0x00130@Program: target is not connected
C28xx_CPU1: Error executing PLL configuration algorithm. Operation cancelled. (0x0)
C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D200@Data: target is not connected
C28xx_CPU1: File Loader: Memory write failed: Unknown error
C28xx_CPU1: GEL: File: C:\Users\LiuJun\workspace_v9\LAN9252_SPI_379\Debug\LAN9252_SPI_379.out: Load failed.
C28xx_CPU1: Error occurred during flash operation: Could not read register PC: target is not connected
C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005F800@Data: target is not connected
C28xx_CPU1: Error occurred during flash operation: Could not write 0x00000@Program: target is not connected
C28xx_CPU1: Error occurred during flash operation: Cannot enable while the target is disconnected
C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005F444@Data: target is not connected
C28xx_CPU1: Error occurred during flash operation: Could not read 0x0007026D@Data: target is not connected
C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005F444@Data: target is not connected
C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005F444@Data: target is not connected
C28xx_CPU1: Error occurred during flash operation: Failed to run target while trying to execute pwrite_en.alg
C28xx_CPU1: Flash operation timed out waiting for the algorithm to complete. Operation cancelled.
C28xx_CPU1: Perform a debugger reset and execute the Boot-ROM code (click on the RESUME button in CCS debug window) before erasing/loading the Flash. If that does not help to perform a successful Flash erase/load, check the Reset cause (RESC) register, NMI shadow flag (NMISHDFLG) register and the Boot-ROM status register for further debug.
C28xx_CPU1: Error occurred during flash operation: Could not read 0x0007026D@Data: target is not connected
C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005F444@Data: target is not connected
C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005F444@Data: target is not connected
C28xx_CPU1: Error occurred during flash operation: Could not read 0x0007026D@Data: target is not connected
C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D200@Data: target is not connected
C28xx_CPU1: Error occurred during flash operation: Could not read 0x5D200@Program: target is not connected
C28xx_CPU1: Error occurred during flash operation: Could not read 0x0007026D@Data: target is not connected
C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005D20E@Data: target is not connected
C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D20E@Data: target is not connected
C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005D20E@Data: target is not connected
C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D20E@Data: target is not connected
C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005D22E@Data: target is not connected
C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005D208@Data: target is not connected
C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D208@Data: target is not connected
C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005D208@Data: target is not connected
C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D208@Data: target is not connected
C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005D222@Data: target is not connected
C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D222@Data: target is not connected
C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D214@Data: target is not connected
C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005D20E@Data: target is not connected
C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D20E@Data: target is not connected
C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D20E@Data: target is not connected
C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D222@Data: target is not connected
C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D200@Data: target is not connected
C28xx_CPU1: Error occurred during flash operation: Could not write 0x00000@Program: target is not connected
C28xx_CPU1: Error occurred during flash operation: Cannot enable while the target is disconnected
C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005F444@Data: target is not connected
C28xx_CPU1: Error occurred during flash operation: Could not read 0x0007026D@Data: target is not connected
C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005F444@Data: target is not connected
C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005F444@Data: target is not connected
C28xx_CPU1: Error occurred during flash operation: Failed to run target while trying to execute pwrite_dis.alg
C28xx_CPU1: Flash operation timed out waiting for the algorithm to complete. Operation cancelled.
C28xx_CPU1: Perform a debugger reset and execute the Boot-ROM code (click on the RESUME button in CCS debug window) before erasing/loading the Flash. If that does not help to perform a successful Flash erase/load, check the Reset cause (RESC) register, NMI shadow flag (NMISHDFLG) register and the Boot-ROM status register for further debug.
C28xx_CPU1: Error occurred during flash operation: Could not read 0x0007026D@Data: target is not connected
C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005F444@Data: target is not connected
C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005F444@Data: target is not connected
C28xx_CPU1: Error occurred during flash operation: Could not write register PC: target is not connected
Are you able to connect to the device/core without loading the code? Which version of CCS are you using?
I modfied the CMD then the faults as follow
C28xx_CPU2: Trouble Removing Breakpoint with the Action "Finish Auto Run" at 0x863d: (Error -1066 @ 0x863D) Unable to set/clear requested breakpoint. Verify that the breakpoint address is in valid memory. (Emulation package 8.1.0.00005)
C28xx_CPU2: Error: (Error -1137 @ 0x0) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 8.1.0.00005)
C28xx_CPU2: Unable to determine target status after 20 attempts
C28xx_CPU2: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging
C28xx_CPU2: GEL: Target must be connected before calling the function
the debug view is present
Have you been able to connect to this device in the past? Is it possible to try putting the device in wait boot mode?
Also, which JTAG debug probe are you using?
NO I've never connect succefully ,i put the design in flash boot mode and can't switch it ,use xds100vs debug
Just to confirm, you see this problem when you are just trying to connect to the device, not when you are loading code?
Also, the test connection passed for both the IR and DR scans?
If you have access to an oscilloscope, could you try probing TDO (yellow), TMS (purple), TCK (blue), and TRST (green) as shown below. The screenshot below was captured using the XDS100, and it was a single-capture triggered on the falling edge of TMS. Could you try doing the same and see if your probed signals look the same when you try to connect?