This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280039C: FLASH_ECC的相关问题(3个)

Part Number: TMS320F280039C
Other Parts Discussed in Thread: UNIFLASH

问题1:STL中FLASH_ECC例程中,使用的是FLASH_ECC的TEST模式作为演示,我想问一下,在我自己的APP程序中,上电自检时,是否需要使用TEST模式?

如果不需要的话,是否只要使能FLASH_ECC及对应的中断即可使能FLASH_ECC检测?

问题2:STL的FLASH_ECC例程中计算了对应FLASH地址,对应数据的ECC值,用于TEST模式下的ECC测试,

那我在我的APP中,需要计算出对应的ECC吗?

是的话,该如何编程呢?

这个ECC校验码是编译时自动计算出来,并写入到对应的ECC_FLASH地址中的吗?

问题3(基于问题2):在TRM的6.9章节中,图6-3所示的红圈部分,

这个ECC码是由APP自己计算生成的?

还是编译器编译完后生成的?

是否是存储在问题2图2的红圈地址中?

以上3个问题,期待得到回复,谢谢。