This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28M35 中dsp与epi通讯



最新的文档里的External Peripheral Interface (EPI)章节中新添加了19.9 C28x Access to EPI。说明c28可以直接访问epi。阅读章节以后产生了以下几个疑问。

1、首先,文档中说明,This means that M3 software must configure the EPI in a particular mode before C28x software can access the external device via EPI.(P 1388)所以需要先在M3中对epi进行配置。对于之后DSP与EPI如何交换信息就没有再提了。

2、RTW的作用是否只是起到阻塞的作用,而且RTW只是存在于M3 与 C28都需要访问epi的时候需要使用 。因为文档中有提到 Once EPI is grabbed by C28x software (GRAB = 1), all accesses to EPI from M3/uDMA will be stalled until EPI is released (GRAB = 0) by C28x software.The RTW feature is only needed in an application where both subsystems (master and control) are accessing EPI and one needs to provide a window for dedicated access to EPI from the control (C28x) subsystem. Otherwise, by default, both subsystems have access to EPI with round-robin arbitration.

3、所以,假如只需要DSP和EPI到底是要如何才能直接交换数据的呢?