This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请问240X的汇编语言程序怎样移植到280x平台上,谢谢!
C24x到C28x平台的汇编代码移植请参考以下文档的610页内容:http://www.ti.com/general/docs/lit/getliterature.tsp?baseLiteratureNumber=spru430&fileType=pdf 。
您好!我下了这篇文档,没有您说的610页。而且里面讲述的是27XX系列代码移植,请问24XX系列汇编代码移植到2803X系列有问题么??
目前新的F2803X都是用CCS5/6编译,外设都有很多改变,所以建议重新用C的架构去编译。移植的工作量太大了。
好的 谢谢了!我们主要使用的芯片是2406A,大部分都是汇编,以为直接移植过去就能直接使用,这样成本应该会很小。我查资料显示,28X系列的架构都是c语言的,移植的成本不见得比重写少。
根据您的经验,
1 有没有和2406A外设各种相同的28XX系列芯片?
2 如果重写,在28XX系列中您给推荐一下吧
谢谢了!
C28XX没有相同的,但是外设都比F2406A强,内核页改成32位的了,推荐F28069,F28075看一下。