This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HVMOTORCTRL+PFCkit LEVEL4A到LEVEL4B切换,AS和BS波形问题



LEVEL4,通过lsw=1修改为lsw=2,clarke1.As和clarke1.Bs(u和v相采样回来再CLARKE变换后的值)的波形

在lsw=1时,为正弦波形;切换到lsw=2,确实一条直线。请厉害的人帮忙解释一下。

如果直接lsw=2,输出波形为正弦,后续来回切换lsw=1或2,输出的还是正弦波形。

正常应该无论怎样,电机稳定运行之后,输出的电流波形都为正弦。

  • The GUI will only work with the ".out" file that is found in the C:\TI\controlSUITE\development_kits\HVMotorCtrl+PfcKit_v1.6\~GUI folder on the 28035 card.  It is really meant for demonstration purposes only.  

    For working with the available demo projects and development, please study the "HowToRunGuide" in the ~Docs folder.