This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

#include "CLAShared.h"



dsp28035的ti例程,我在 DSP2803x_Device.h添加#include "CLAShared.h"为何编译会出现错误啊

#include "DSP2803x_PieCtrl.h"            // PIE Control Registers
#include "DSP2803x_PieVect.h"            // PIE Vector Table
#include "DSP2803x_Spi.h"                // SPI Registers
#include "DSP2803x_Sci.h"                // SCI Registers
#include "DSP2803x_SysCtrl.h"            // System Control/Power Modes
#include "DSP2803x_XIntrupt.h"           // External Interrupts
#include "CLAShared.h"

还有一个奇怪现象

本来原程序中Example_2803xClaAdcFir.c有头文件--#include "CLAShared.h"    正常

#include "DSP28x_Project.h" // includes all of the header files and defines used in the
                            // example projects   
#include "CLAShared.h"      // includes all of the shared variables (shared between
                            // C28x C source and CLA assembly code)

为何我在DSP2803x_GlobalVariableDefs.c中添加--#include "CLAShared.h"  就异常了?

#include "DSP2803x_Device.h"     // DSP2803x Headerfile Include File
#include "CLAShared.h" 

编译完提示结果:

"DSP2803x_GlobalVariableDefs.c", line 15: fatal error: could not open source file "CLAShared.h"
1 fatal error detected in the compilation of "DSP2803x_GlobalVariableDefs.c".
Compilation terminated.

>> Compilation failure