This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

cla.asm 32位/16位变量区别



我应用的是dsp f28035.我现在定义了两个变量,都是32位浮点。我在cla,asm中运行,32位的值_CputoCla._claa不随_CputoCla._clab的变化而变化,一直是初始值,但是_VoltFilt是可以的。_VoltFilt是定义的16位整形。难道是因为32位和16位的区别吗?cla不是可以用来32位的吗

我在main.C主函数中初始化:

CputoCla._clab=25000.0; 
CputoCla._claa=800.0;

在CLA.asm中运行以下:

;;;;;;;;;;;;;;;;;;;;;;;
MMOV32 MR0,@_CputoCla._clab
MMOV32 @_CputoCla._claa,MR0
MNOP ;3 Wait till I8 to read result
MNOP ;4 Wait till I8 to read result
MNOP ;5 Wait till I8 to read result
MNOP ;6 Wait till I8 to read result
MNOP

;;;;;;;;;;;;;;;;;;;;;;
;MMOVF32 MR0,#105.6
MF32TOUI16 MR2, MR0 ; Get back to Uint16 value
MMOV16 @_VoltFilt, MR2

现在的问题是_VoltFilt可以正常的为2500,而_CputoCla._claa为何不等于2500还是原来的初始值_CputoCla._clab呢?请大侠来帮帮忙。

  • 补充

    又如:我现在又定义了两个变量CputoClaAAA和CputoClaBBB,也还是出现类的情况。

    #pragma DATA_SECTION(CputoClaAAA,"CpuToCla1MsgRAM");
    #pragma DATA_SECTION(CputoClaBBB,"CpuToCla1MsgRAM");

    Uint16 CputoClaAAA,CputoClaBBB;

    在main中初始化

    CputoClaBBB=1258;
    CputoClaAAA=2536;

    MMOVZ16 MR0,@_CputoClaAAA
    MMOV16 @_CputoClaBBB,MR0
    MNOP ;3 Wait till I8 to read result
    MNOP ;4 Wait till I8 to read result
    MNOP ;5 Wait till I8 to read result
    MNOP ;6 Wait till I8 to read result
    MNOP

    运行后CputoClaBBB=1258为何还是不能更新为CputoClaAAA的值2536呢,如何让_CputoClaBBB跟随_CputoClaAAA变化呢?网大侠支招。

  • 难道是因为CputoClaAAA,CputoClaBBB都在CpuToCla1MsgRAM这个cpu区间,它们之间不能相互传递值吗,不应该这样啊

  • _VoltFilt的值能够跟随A4改变,而CputoClaBBB不能,就是因为_A4 和CputoClaBBB是同一区间,_A4 和_VoltFilt不在同一区间的缘故吗

    在这定义

    #pragma DATA_SECTION(A,          "CpuToCla1MsgRAM");

    #pragma DATA_SECTION(CputoClaBBB,"CpuToCla1MsgRAM");

    而#pragma DATA_SECTION(VoltFilt,   "Cla1ToCpuMsgRAM");

    #if LOWPASS
    float32 A [FILTER_LEN] = {625, 100, 200, 300, 2000};
    #elif HIGHPASS
    float32 A [FILTER_LEN] = {625, 100, 200, 300, 2000};//T{0.0625L, 0.25L, 0.375L, 0.25L, 0.0625L}
    #endif

    MMOV32 MR0,@_A4
    MF32TOUI16 MR1,MR0
    ; MMOVZ16 MR0,@_CputoClaAAA
    MMOV16 @_CputoClaBBB,MR1
    MMOV16 @_VoltFilt, MR1

    这个问题困扰好久了,请来帮助我,在这多谢了。