This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377D: 2837xD之IPC通信(共享内存)

Part Number: TMS320F28377D
Other Parts Discussed in Thread: CONTROLSUITE

跑的例程是ti公司的controlSUITE里找到的。位置:“器件”->“Delfino F2837xD”->“代码示例”->“所有双核示例”->“RAM_management”

跑例程 显示正在运行,但是板子上面没有反应。运行成功的话应该是要两个led灯交互闪烁的。

代码来源放到这:代码来源

其中

extern uint16_t isrfuncLoadStart;

extern uint16_t isrfuncLoadEnd;

extern uint16_t isrfuncRunStart;

extern uint16_t isrfuncLoadSize;

这一段代码的来源

SECTIONS
{

/* Allocate program areas: */

isrfunc : LOAD = RAMD0 | RAMLS0 | RAMLS1 | RAMLS2 | RAMLS3 | RAMLS4,
RUN = RAMGS15,
LOAD_START(_isrfuncLoadStart),
LOAD_END(_isrfuncLoadEnd),
RUN_START(_isrfuncRunStart),
LOAD_SIZE(_isrfuncLoadSize),
PAGE = 0

}