This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求助,,,大家帮我看看我的28027 i2c模块程序哪里出错了



程序的功能是给24c02   第0x00个字节写入0x20,然后再读回到变量b中
#include "DSP28x_Project.h"

#define I2C_SLAVE_ADDR        0x50
#define I2C_NUMBYTES   15
#define I2C_EEPROM_HIGH_ADDR  0x00
#define I2C_EEPROM_LOW_ADDR   0x00
void  I2CA_SendData(void);
void  I2CA_ReceiveData(void);

void main(void)

{

        InitSysCtrl();
        InitI2CGpio();
        DINT;
        InitPieCtrl();

        IER = 0xffff;
        IFR = 0x0000;

        InitPieVectTable();
        InitI2C();
        I2CA_SendData();
        I2CA_ReceiveData();
        while(1);
}

void  I2CA_SendData(void)
{
        Uint16 i;
    I2caRegs.I2CSAR = I2C_SLAVE_ADDR;                         //Set slave address
    I2caRegs.I2CCNT = 1 + 1;                         //Set count to 5 characters plus 2 address bytes
    I2caRegs.I2CDXR = 0x02;//Send eeprom high address
    I2caRegs.I2CMDR.bit.TRX = 1;                                 //Set to Transmit mode
    I2caRegs.I2CMDR.bit.MST = 1;                                 //Set to Master mode
    I2caRegs.I2CMDR.bit.FREE = 1;                                //Run in FREE mode
    I2caRegs.I2CMDR.bit.STP = 1;                                 //Stop when internal counter becomes 0
    I2caRegs.I2CMDR.bit.STT = 1;                                 //Send the start bit, transmission will follow

    while(I2caRegs.I2CSTR.bit.XRDY == 0);                 //Do nothing till data is shifted out
    I2caRegs.I2CDXR = 0x20;                          //Send eeprom low address
}

void  I2CA_ReceiveData(void)
{
        Uint16 i;
        char b[20];
        b[0]=0;
    I2caRegs.I2CSAR = I2C_SLAVE_ADDR;                         //Set slave address
    I2caRegs.I2CCNT = 1;                                                 //Set count to 2 address bytes
    I2caRegs.I2CDXR = 0x00;                        //Send eeprom high address
    I2caRegs.I2CMDR.bit.TRX = 1;                                 //Set to Transmit mode
    I2caRegs.I2CMDR.bit.MST = 1;                                 //Set to Master mode
    I2caRegs.I2CMDR.bit.FREE = 1;                                //Run in FREE mode
    I2caRegs.I2CMDR.bit.STP = 0;                                 //Dont release the bus after Tx
    I2caRegs.I2CMDR.bit.STT = 1;                                 //Send the start bit, transmission will follow

    I2caRegs.I2CCNT = 1;                                //read 5 bytes from eeprom
    I2caRegs.I2CMDR.bit.TRX = 0;                                 //Set to Recieve mode
    I2caRegs.I2CMDR.bit.MST = 1;                                 //Set to Master mode
    I2caRegs.I2CMDR.bit.FREE = 1;                                //Run in FREE mode
    I2caRegs.I2CMDR.bit.STP = 1;                                 //Stop when internal counter becomes 0
    I2caRegs.I2CMDR.bit.STT = 1; //Repeated start, Reception will follow
    b[0] = I2caRegs.I2CDRR;
    while(1);
}

void InitI2C(void)
{
    // Initialize I2C-A:
        I2caRegs.I2CSAR = 0x0050;        // Slave address - EEPROM control code
        I2caRegs.I2CPSC.all = 6;       // Prescaler - need 7-12 Mhz on module clk
        I2caRegs.I2CCLKL = 10;           // NOTE: must be non zero
        I2caRegs.I2CCLKH = 5;            // NOTE: must be non zero
         I2caRegs.I2CIER.bit.ARDY = 0;
         I2caRegs.I2CIER.bit.XRDY = 0;
        I2caRegs.I2CFFTX.all = 0x0000;   // Disable FIFO mode and TXFIFO
        I2caRegs.I2CFFRX.all = 0x0000;   // Disable RXFIFO, clear RXFFINT,

          I2caRegs.I2CMDR.all = 0x0020;    // Take I2C out of reset
                                            // Stop I2C when suspended


}