This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28335 pwm cpu

28335输出pwm波时需要cpu参与嘛?

  • 输出产生PWM不需要CPU参与,但是配置PWM模块,提供下一个周期和比较数据需要CPU提供。

  • f28335能否实现这样的功能:

    1、输出两路时钟信号,占空比50%,频率精确且独立可调;

    2、时钟信号输出后,可在指定时刻进行两路同时A/D采集。

  • 可以用2个PWM模块来实现输出2路信号。

    建议考虑2806x因为28335中没有PWM的周期高精度功能,也就是说2806x的频率精度会比28335的高。

    第二个功能可以实现。