This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

使用TMS32OF2812,将CCS3.1下正常的在线烧写flash工程移植到CCS4.2上遇到的问题,求助各位专家和高手们?

在CCS3.1下,升级工程updata和主应用工程app能互相引导配合,实现在线烧写flash功能,长期运行过,在线升级一直没问题。主要过程是:app.Out烧写至CDE区,updata.out烧写至A区,程序正常启动时由updata程序引导至0x3E8000即app程序入口,需要升级时由app程序跳转至0x3F7FF6开始运行updata程序。

最近更换了xds560v2的仿真器,想将平台迁移至CCS4.2上,移植工程编译通过了,主应用工程app单独运行正常,但配合升级工程updata时出现了不能引导app程序的问题,后经反汇编单步调试,发现程序跳转至0x3E8000后进入死循环找不到app程序的_c_int00和mian(),对比两个平台生产的map文件发现,经过CCS4.2编译后的app程序的_c_int00地址变化了,而且不是个固定值,跟之前CCS3.1下编译后_c_int00固定在地址0x3E8000的结果不一样,自己怀疑是这个原因造成程序引导失败,但不知道怎么解决?查资料说_c_int00在rst2800.lib中定义,尝试分别加载rst2800.lib和rst2800_ml.lib两种库结果都一样,为什么移植到CCS4.2编译后_c_int00地址变化了?移植后需要更改CMD文件吗?或是编译连接选项设置有问题吗?被这个问题困扰很久了,请大家帮帮忙吧,非常感谢!