This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

2812中SCI通信问题

2812的SCI接RS485电平转换芯片MAX3082,2812发送数据出来电脑串口助手能收到,但是电脑串口发送出来后,差分信号就只有单边电平了,取掉板子与电脑的通信线,测量插在电脑串口上的转换器,又是差分信号,请问大侠们,这是个神马情况,没头绪了

  • 2812能上发   上发的时候你看了没有     SCI到485后  是不是差分信号

    你的通信线是MAX3082和PC机之间的吧     会不会是有一路信号短路等情况

    只有一路差分信号有可能是能收到的

  • 2812上发的时候确实是差分信号,通信线就是连接PC和3082的,