This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
paper連結: www.ti.com/.../spry212.pdf
如題,在此篇TI的paper 於3.1節說明了提供Resolver to Digital Conversion的硬體電路。
1. 文中提到解角器是由 峰對峰值為10V的sine波作為一次側的輸入,想請問range是否為 0~10V 的sine波? (因為OPA2009的限制電壓為0~15V)
2. 假設解角器的input為 0~10V 的sine波,感應出來的output 大小range又為何?? paper似乎沒有提到解角器的轉換率。
3. 解角器input為正電壓準位,代表著感應出來的output也會為正電壓準位,但又為何需要經由TLV2772提升1.65V電壓準位?
想請高手幫忙解答, 謝謝~
Kevin Huang
Kevin,
1、Resolver也就是你说的转角器输入的值,通常是一个-X到+X的sine波,虽然OPA2009的限制电压是0~15V,但根据文档中的Figure 5: Hardware schematic diagram,电路的输出 to Resolver Pramiry应该是一个-5V到+5V的sine波,我没有仔细分析电路,你需要确认一下。
2、解角器的输出应该不会是 -1.65~+1.65,这里的这个值应该是放大电路作用后的效果