This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

2812始终不运行



您好,我是刚刚接触TI的产品,使用的是2812,我的CPU系统是做过PCB板的,程序过程中的运行环境为CCS3.3,遇到情况是:

程序通过JTAG口进行仿真烧写到内置RAM中时,经过load program后,绿箭头指在 3FFC00 28AD MOV     @SP,#0x0400 上,但运行程序后经过run和halt后绿箭头始终停留在这句话上。请问是怎么回事?

PS:该程序在2812开发板上运行正常

  • Load基于RAM的程序到片上运行,需确定你的.cmd文件是配置到RAM,之后进行load program --> reset --> restart --> go main --> run.

  • 楼主用下面的例程试试吧:

    www.ti.com.cn/.../sprc097

  • resetCPU时,Error connecting to the target: Error 0x00000204/-1147 Error during: Register, OCS,  It appears that the target is being held in reset.  If this is a multi-core system, the master CPU may not be releasing the DSP from reset.  Please check your configuration in CCSetup and/or your GEL file to ensure that nothing is blocking the DSP from being released from reset   Sequence ID: 0 Error Code: -1147 Error Class: 0x00000204

  • RESET CPU 时,Error connecting to the target: Error 0x00000204/-1147 Error during: Register, OCS,  It appears that the target is being held in reset.  If this is a multi-core system, the master CPU may not be releasing the DSP from reset.  Please check your configuration in CCSetup and/or your GEL file to ensure that nothing is blocking the DSP from being released from reset   Sequence ID: 0 Error Code: -1147 Error Class: 0x00000204