dsp28035内部含有cla模块,cla中有_Cla1Task1-_Cla1Task8,共8个任务,我想问下,进入_Cla1Task1-_Cla1Task8的频率时多少,是28035的时钟觉得的吗,我现在用的是60MHZ,那_Cla1Task1-_Cla1Task8工作频率就是60MHZ吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
dsp28035内部含有cla模块,cla中有_Cla1Task1-_Cla1Task8,共8个任务,我想问下,进入_Cla1Task1-_Cla1Task8的频率时多少,是28035的时钟觉得的吗,我现在用的是60MHZ,那_Cla1Task1-_Cla1Task8工作频率就是60MHZ吗?
是的,你现在用60MHz,那么 CLA(control law accelerator)的每一个任务最大工作频率不会超过60,它们是并行的,具体的参考请到TI官网下载CLA参考指南,里面有详细的用法。具体的内容我也不太了解,希望遇到问题首先去翻翻user guide。 希望能帮到你。
cla的频率和cpu主频一致,具体1-8的任务的执行频率时应该按照其各自的触发频率有关是吧?
任务触发机制:
¾ C28x CPU 通过 IACK 指令来触发;
¾ Task1~Task7:对应 ADC 或 ePWM 模块中断。例如:
¾ Task1:ADCINT1 或 EPWM1_INT;
¾ Task2:ADCINT2 或 EPWM2_INT;
¾ Task7:ADCINT7 或 EPWM7_INT;
¾ Task8:ADCINT8 或 CPU Timer0 来触发的任务。