用这个程序跑了一遍,然后用XDS510再也连接不上F28335了,故障显示芯片locked,很奇怪,请问如何处理????
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
用这个程序跑了一遍,然后用XDS510再也连接不上F28335了,故障显示芯片locked,很奇怪,请问如何处理????
将启动设置为0011(87-86),可以连接上,但是出现以下错误:
1、可以确认ccxml文件芯片选择没错,它怎么就检测芯片不匹配呢?
C28xx: Flash Programmer: Warning: The configured device (TMS320F28335), does not match the detected device (). Flash Programming operations could be affected. Please consider modifying your target configuration file.
C28xx: GEL Output:
ADC Calibration not complete, check if device is unlocked and recalibrate.C28xx: GEL Output:
ADC Calibration not complete, check if device is unlocked and recalibrate.C28xx: GEL Output:
ADC Calibration not complete, check if device is unlocked and recalibrate.C28xx: GEL Output:
ADC Calibration not complete, check if device is unlocked and recalibrate.C28xx: Breakpoint Manager: Retrying with a AET breakpoint
C28xx: Trouble Setting Breakpoint with the Action "Finish Auto Run" at 0x94ff: (Error -1066 @ 0x94FF) Unable to set/clear requested breakpoint. Verify that the breakpoint address is in valid memory. (Emulation package 5.1.232.0)
C28xx: Can't Run Target CPU: (Error -1140 @ 0x0) Lost debug connection to device. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 5.1.232.0)